Delete a custom tag
You can delete any custom tag that is not associated with a device type.
- If the tag is associated with a device type, you must first deselect the tag:
- Change the option to Edit Existing and display the tag you want to delete.
- Click Display Associated Device Types to display all device types that include this tag. Make a note of the device types.
- Return to the Add/Edit Device Type screen. For each device type listed, deselect the tag that you want to delete.
Continue deleting the tag:
- Open the Add/Edit Custom Tags screen.
- In the Custom Tag Options box, click Delete Existing.
- From the drop-down menu, choose the tag you want to delete.
- Click Delete.
- Click Yes to confirm the deletion.
- Click Save to save the change, or click Save & Exit to save changes and close the screen.